Options in the Graphic Display Scaling dialog box
The following table shows the options in the
Graphic Display Scaling
dialog box.Options | Descriptions |
|---|---|
Scale graphic displays | Select this check box to let displays be scaled to match whatever changes you have made. |
Scale the font size used by objects | Select this check box to scale the text on graphic objects. The new font size is determined as a percentage of the original font's height. Text objects will be scaled only if the SizeToFit property is set to False .Fonts used by ActiveX controls will not be scaled. |
Scale the border sizes used by objects | Select this check box to scale object's borders. The new border width is calculated as a percentage of the original. New border widths with a floating point value greater than 1 will be rounded down to the nearest integer. Border widths with a floating point value less than 1 will be rounded up to 1. |
Scale the images in the Images folder | Select this check box to scale the size of images in the Image folder as a percentage of the original.The images will maintain the same height and width ratio as the original. If the project window size is changed and the vertical and horizontal scaling factors are not the same, the smallest scaling factor will be applied to both height and width. |
Scale the offsets used in animations | Select this check box to scale the Horizontal offset and the Vertical offset pixels as a percentage of the original for the following animations:
|
Provide Feedback