Firewall ports and URL access

To ensure that FactoryTalk Updater can access the Product Compatibility and Download Center (PCDC) data and download the latest patches, you must add the following URLs to the firewall exception list:
When using the server installation:
  • api.rockwellautomation.com
When using the client installation:
  • login.rockwellautomation.com
  • netstorage.rockwellautomation.com
FactoryTalk Updater deployment - with ports
During operation, FactoryTalk Updater opens these firewall ports on the server:
Server Firewall Ports
Port Type
Port Number
Description
TCP
808
Allows the FactoryTalk Updater Agent and FactoryTalk Updater Client to connect to the FactoryTalk Updater Server.
TCP
60129
Allows access to the web-based FactoryTalk Updater Client.
UDP
137
Ping computer names.
Network-Echo Request (ICMPv4-In)
Allows one computer to contact or ping another computer to test network communications.
During operation, FactoryTalk Updater opens these firewall ports on the agent:
Agent Firewall Ports
Port Type
Port Number
Description
TCP
30064
Allows access to the agent service to change the server address.
UDP
3702
Allows Auto Discovery broadcast message.
UDP
137
Used to ping computer names.
Network-Echo Request (ICMPv4-In)
Allows one computer to contact or ping another computer to test network communications.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal