Find, group, and add devices for monitoring
- To find machines, selectFind Machines, and perform one of the following actions:
- To scan the network and find machines automatically, selectAuto Discover.
- To search for machines using an IP address or a range of addresses, selectManual.
- To search for a specific machine, selectSingleand enter the machine's IP address.
- To search for machines within a range of IP addresses, selectRangeand enter the range of IP addresses.
- To locate machines that are not connected to the current server, selectFIND MACHINES.The found machines appear in a table that lists each machine's name and IP address. Found machines are ungrouped by default.
- To assign a machine to an existing group, select
next to the group name and select a group. Machines left ungrouped appear only in theAll Machineslist. - To add multiple machines to the same group, select the checkboxes for the machines, select
in the Group column, and then select a group. - To assign a machine to an existing group, select
beside the group name and select +, type the group name and press Enter. - To add machines to the main page, select the checkbox for the machines and selectADD MACHINES.
- To edit a group name or delete a group, select
in the Group column, hover over a group, and select the Edit icon
to edit the group name or select
to delete the group. All machines in a deleted group revert to ungrouped.
Provide Feedback