Tag values from OPC UA Servers do not update or have bad quality
Possible cause and solution:
- TheFactoryTalk LinxOPCUA Connector orOPCUA Server does not have network connectivity.Verify network continuity between theFactoryTalk LinxOPCUA Connector workstation andOPCUA Server.
- TheOPCUA Server software is no longer running, has crashed, or its host computer is shut down or restarting.Verify the host PC is running. UseWindowsServices to determine if theOPCUA Server software is operating normally.
- TheOPCUA Server is unable to connect to one or more data sources.Verify network continuity between theOPCUA Server and each data source.Verify the data source is running.View theFactoryTalkDiagnostic Log for one or more communication errors. Use the failingOPCUA node ID or tag to identify the affected host data source.
- TheFactoryTalk LinxOPCUA Connector has an outdated list of tag names. In, a data error appears for each node ID theFactoryTalk DiagnosticsLogFactoryTalk LinxOPCUA Connector cannot access. Error codes may include "Bad", "BadCommunicationError", "BadDeviceFailure", "BadTimeout", "UncertainInitialValue", or "UncertainSensorNotAccurate". Multiple tags may not update or may show bad quality even if only one tag name is outdated.Refresh tag names for theOPCUA Server and restart the OPC UA Connector service:
- InExplorer, right-click an existingFactoryTalk LinxOPCUA Connector, then selectProperties.
- In, selectFactoryTalk LinxOPCUA ConnectorOPC UA Servers.
- Highlight anOPCUA Server, then selectRefresh Tag Names.
- InRefresh Tag Names, selectContinue with reset.IMPORTANT:The FactoryTalk Linx OPC UA Connector service restarts.FactoryTalk clients do not receive OPC UA tag values from any OPC UA Server connected to this FactoryTalk Linx OPC UA Connector until the reset is complete.
Provide Feedback