Refresh the tag names

FactoryTalk Linx
OPC UA Connector caches folder names, tag names, and tag data types from each connected OPC UA Server. The cache operation occurs once, when the OPC UA Server is added to the OPC UA Connector. If the folder names, tag names, or tag data types in the OPC UA Server change, manually refresh tag names to help ensure that the OPC UA Connector presents the correct information to
FactoryTalk
applications.
The cache file is stored on the OPC UA Connector host computer at
C:\ProgramData\Rockwell\OpcUaConnector\RnaUaClientDataProvider\cache\
.
After refreshing tag names, there is a delay before all server tags appear in the
FactoryTalk
Tag Browser. The delay time is dependent on OPC UA Server specifications, network specifications, and the data model of the tags provided to the OPC UA Connector. Monitor the
@OPC_NamespaceCacheUploadCompleteStatus
predefined diagnostic item of the server to identify when the tag name upload has completed.

To refresh tag names from an OPC UA Server

  1. In, select
    OPC UA Servers
    .
  2. On
    OPC UA Servers
    , select an OPC UA Server, and then select
    Refresh Tag Names
    .
  3. In , select a reset option:
    Button
    Description
    Continue with reset
    The OPC UA Connector refreshes the list of tags from the selected OPC UA Server.
    The OPC UA Connector service restarts.
    FactoryTalk
    clients do not receive OPC UA tag values from any OPC UA Server connected to this OPC UA Connector until the reset is complete.
    Continue without reset
    The OPC UA Connector refreshes the list of tags from the selected OPC UA Server.
    The OPC UA Connector service does not restart.
    FactoryTalk
    clients continue to receive tag values from all OPC UA Servers based on the previously cached tag lists. Modifications to the OPC UA Server's tag list are ignored until a reset is performed.
    Cancel
    The OPC UA Connector does not refresh the list of tags from the OPC UA Server.
    The OPC UA Connector service does not restart.
    FactoryTalk
    clients continue to receive tag values from all OPC UA Servers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal