Design (Local) and Runtime (Target) tabs on the Communication Setup editor
When used with
FactoryTalk View ME
, FactoryTalk Linx
manages two separate sets of topology data and keeps track of the shortcut references into both sets as described below:- the set on the local workstation, which is used to build and test applications (Communication Setupeditor, Design (Local)tab. This was called the Local tab in versions prior to CPR 9.)
- the set that will be deployed to the actual target device, for example, aPanelView Plus(Communication Setupeditor, Runtime (Target)tab. This was called the Target tab in versions prior to CPR 9.)
A single shortcut can reference a different device in each topology data set.
To open the
Communication Setup
editor from the Explorer, double-click Communication Setup
under the FactoryTalk Linx
data provider. The two tabs on the editor, Design
(Local) and Runtime
(Target), provide different functions and perspectives for setting up communications.
TIP:
The
Runtime
(Target)
tab shortcuts are the only shortcuts copied into the runtime (.mer) file. You must either manually add the shortcuts to the Runtime (Target)
tab, or copy the Design (Local)
tab configuration to the Runtime (Target)
tab before you create the runtime application to be able to use the shortcuts. Note that if you copy the configuration to the Runtime (Target)
tab, you should verify that the shortcuts reference the correct devices.Design (Local) tab | Runtime (Target) tab |
|---|---|
Displays a view of the system from this workstation's (the development computer's) perspective. That is, it reflects the view of the topology from the FactoryTalk Linx server on this workstation. The FactoryTalk Linx Design (Local) tab is similar to RSLinx Classic 's online view of the system. | Displays (offline) the offline configuration from the perspective of the target HMI device that will be running the application and comprises the topology that will be loaded into the target device. |
Allows you to create and test your application on this workstation before you actually deploy the application to a target device. | Allows you to create the runtime application that will be delivered to and activated on a deployment target such as a PanelView Plus terminal or a FactoryTalk View ME Station desktop computer. |
Is online enabled, which means it is capable of browsing attached networks and automatically discovering devices when you click on a node (whether a device or driver) or select Start Browsing from the context menu on that node. The online mode and browse status indicator appear at the bottom of the tab. | Is an offline configuration tool only, which requires you to right-click and manually add drivers, devices, and shortcuts. The offline mode status indicator appears at the bottom of the tab. |
As you add drivers, devices, and shortcuts to the Design (Local) tab, this information is stored to a file and is used for testing the application. The communications you configure on the Design (Local) tab are not used for the runtime project unless you copy them to the Runtime (Target) tab before the runtime application is created. | The runtime tab data, along with other information, is written to a .mer file when you click Application > Create Runtime Application . The .mer file is deployed when you use the File Transfer Utility and select a target (such as a PanelView 700). |
Provide Feedback