Communication Setup editor, Runtime (Target) tab (FactoryTalk View ME)
How do I access the Communication Setup editor?
From the
Explorer
, under the FactoryTalk Linx
data server, double-click Communication Setup
.For
FactoryTalk View ME
applications, the Communication Setup editor consists of a Device Shortcuts
area, a Runtime (Target)
tab, a Shortcut Properties
table, and a status message area.Use the
Runtime (Target)
tab to:- Add drivers
- Add devices
- Set up driver and device properties
- Set up device shortcuts for use in a configurationTIP:This tab was calledTargetin versions prior to CPR 9.
Provide Feedback