Language switching for alarm messages

You can use language switching to view user-defined text strings in multiple languages at runtime in
FactoryTalk View
SE Client applications. This includes tag-based alarm messages created in the
Alarm and Event Setup Editor
and device-based alarm messages created in the
Logix Designer
application.
When the Alarm and Event Setup editor opens in
FactoryTalk Administration Console
, alarm messages show in the default language defined for the application. If a message string does not exist in the default language, a question mark (
?
) is shown.
When the
Alarm and Event Editor
opens in
FactoryTalk View Studio
, alarm messages show in the language selected during startup of the
FactoryTalk View
SE application. If alarm messages are not defined in the specified language, alarm messages show in the default language defined for the application. If a message string does not exist in the default language a question mark (
?
) is shown.
Application Settings
The Tag Alarm and Event Server checks the following application settings in
FactoryTalk View
at start up:
  • Default language for the application.
  • Display undefined strings using the default language check box.
If you make changes to either of these settings while a Tag Alarm and Event Server is running, you must restart the computer that is running the alarm server or the alarm server continues to use the previous application settings.
If the
Display undefined strings using the default language
check box is selected in
FactoryTalk View
, alarms with undefined alarm messages will be logged using the message strings from the default language configured for the application.
If an alarm message is undefined for the default language, or if the
Display undefined strings using the default language
check box is not selected, the following string will be used for the message: "Message not defined for language:
LanguageName
". For example, "Message not defined for language: French (Canada), fr-CA".
For more information on setting up language switching in
FactoryTalk View
SE, see the
FactoryTalk View
User's Guide
, available from the
Help
> Online Books
menu in
FactoryTalk View Studio
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal