Use tag-based alarm monitoring

Tag-based alarm monitoring uses a software-based Tag Alarm and Event Server to provide a generic method of capturing alarm and event information across heterogeneous systems. Software-based Tag Alarm and Event Servers monitor controller tags for alarm conditions through data servers and publish event information for display and logging. This is in contrast to device-based alarm monitoring, where the alarm notification source is a physical device, namely a
Studio 5000
controller.
Tag-based alarm monitoring is used for
Studio 5000
controllers,
PLC-5
, and
SLC 500
devices communicating through
Rockwell Automation
Device Servers (
FactoryTalk Linx
), or for third-party controllers communicating through OPC data servers.
Set up tag-based alarm monitoring to monitor alarms from
PLC-5
or
SLC 500
controllers, third-party controllers communicating through OPC data servers, and
Studio 5000
controllers that have not been programmed with the
Studio 5000
Logix Designer
application.
  • Use either
    FactoryTalk
    Administration Console or
    FactoryTalk View Studio
    to add a Tag Alarm and Event Server to the application.
  • Use the
    Alarm and Event Setup
    dialog box to set up conditions for triggering alarms.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal