Security permissions: perform alarm-specific commands
Use the tables below to determine which security permissions are required to perform alarm-specific or event-specific operations.
Perform alarm-specific or event-specific operations from within graphic objects | ||
|---|---|---|
To do this | Explorer window object | You need these permissions |
Acknowledge alarms | Area where alarm resides | Alarming > Acknowledge |
Enable or disable alarms | Area where alarm resides | Alarming > Enable/Disable |
Reset latched alarms | Area where alarm resides | Alarming > Reset |
Suppress or unsuppress alarms | Area where alarm resides | Alarming > Suppress |
Suppress or unsuppress diagnostic events | Area where alarm resides | Automatic Diagnostics > Suppress |
Run alarm-specific commands from control tags | |
|---|---|
To do this | You need these permissions |
OperAck - acknowledge digital alarm | Common > Tag Write Alarming > Acknowledge |
OperAckAll - acknowledge Level or Deviation alarm | Common > Tag Write Alarming > Acknowledge |
OperEnable - enable alarm | Common > Tag Write Alarming > Enable/Disable |
OperDisable - disable alarm | Common > Tag Write Alarming > Enable/Disable |
OperReset - reset latched alarm | Common > Tag Write Alarming > Reset |
OperSuppress - suppress alarm | Common > Tag Write Alarming > Suppress |
OperUnsuppress - unsuppress alarm | Common > Tag Write Alarming > Suppress |
AlarmCountReset - clear alarm count | Common > Tag Write |
Provide Feedback