Security permissions: import and export alarm definitions
Use the table below to determine which security permissions are required to import and export alarm definitions.
To do this | Explorer window object | You need these permissions |
|---|---|---|
Import alarm definitions or messages | Area | Common > Read Common > Write Alarming > Enable/Disable |
Export alarm definitions or messages | Area | Common > Read |
Provide Feedback