Secure features of a single product
To restrict access to one or more features of a single
FactoryTalk
property, use Feature Security Properties
. To secure features of a single product
- Log on to theFactoryTalk Directory.
- InFactoryTalk Administration ConsoleExplorer, expandSystem>Policies > Product Policies.
- In theProduct Policiesfolder, expand the folder for the product.
- Right-clickFeature Securityand selectProperties.
- InFeature Security Properties, select the row containing the feature. A description of the feature appears at the bottom of the window.
- Configure the security settings for the feature:
- If the product policy contains settings that are configured using lists, configure the settings, selectOK, and skip the rest of the steps.
- If the product policy is not configured using lists, in the column on the right, selectBrowse(...) besideConfigure Security.
- UseConfigure Securable Actionto select the users or user groups that have permission to access the feature and selectOK.
- Repeat steps 4-6 as needed to configure the features that make up the product policy.
- SelectOK.
Provide Feedback