Validate a policy model

Validate a policy model to confirm that all devices are operational and have network access.
  1. From the toolbar, select
    Validate
    and then select either:
    • CIP Security protocol
      to validate connections between
      CIP Security
      system components.
      For more information, see CIP security policy.
    • OPC UA protocol
      to validate connections between
      OPC UA
      system components.
      For more information, see OPC UA security policy.
    • (administrators only)
      CIP Redundancy (IP Swapping Mode)
      to validate connections between Redundant Chassis Pairs.
      For more information, see Redundancy system.
    TIP: You can stop the validation process at any time by pressing
    STOP VALIDATION
    in the status bar.
    Results
    display any potential information messages, warnings, or errors.
  2. (optional) Save the validation results by selecting
    Save
    .
If devices reject incoming connections with error
0x090C
due to a certificate chain issue or report insufficient file space, do the following:
  1. Delete the problematic devices from the policy model. See Delete a device.
  2. Deploy the policy model.
  3. Add the devices back to the policy model. See Add a device.
  4. Validate the policy model again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal