Mobile connectivity
Securely manage the supported
PowerFlex®
devices through the
external mobile application
.Overview
To set mobile connectivity for the supported devices, provide and set a Pre-Shared
Key (PSK) and PSK ID, and then enter those values into the
mobile application
. Deploy the security policy model to enable the device
to connect with the mobile application
. For more information, see Set PSK for mobile connectivity.
TIP:
For security reasons, PSK keys are only visible during the set-up.
You cannot view PSK keys after the PSK keys are set for mobile
connectivity.
Once you set PSK and PSK IDs for mobile connectivity, you can either reset or delete
the PSK and PSK ID values, or rename the PSK ID value. For more information, see:
Devices with PSK configured for mobile connectivity display in the
Mobile
Connectivity
columns in the tables view. For more information, see
Security policy model tables.
TIP:
Use the
Mobile Connectivity
column or table filters to find
devices configured for mobile connectivity.Compatibility
Mobile connectivity supports these
PowerFlex®
750-Series via Embedded EtherNet/IP devices with firmware revision 12.00 or later in zones with secure communication and certified authentication:
- PowerFlex®755TL drive
- PowerFlex®755TM common bus inverter
- PowerFlex®755TM regenerative bus supply
- PowerFlex®755TR regenerative drive
- PowerFlex®755TS drive
TIP:
In
FactoryTalk Policy Manager
, you cannot cut, copy, or paste devices configured for mobile connectivity. You can move such devices between zones with secure communication and certified authentication.Provide Feedback