Zone CA certificates regeneration
Regenerate Certificate Authority (CA) certificates for zones. Apply the
regenerated zone CA certificates to devices in these certified zones.
TIP:
Regenerating CA certificates is a recommended
security practice that helps prevent attacks by forcing key rotation across the security
policy model
In
FactoryTalk Policy Manager
, administrators can regenerate zone CA certificates and
apply them to CIP Security
capable devices and OPC UA
capable devices. Regenerated CA certificates
apply to devices in certified zones after a security policy model deployment.To regenerate CA certificates, see Regenerate zone CA certificates.
For settings reference, see CA Certificate Management and Policies.
Provide Feedback