Back up a policy model

Back up
FactoryTalk System Services
to save a copy of the policy model and its associated certificates.
  1. Open the command prompt as an Administrator.
  2. In the command prompt, change the directory by running:
    cd "C:\Program Files (x86)\Rockwell Software\FactoryTalk System Services"
  3. Create a password-protected backup file by running:
    FtssBackupRestore -B -P "
    password
    "
    Where
    password
    is a password used to encrypt the backup file.
    TIP: Quotation marks for
    password
    are optional. The
    password
    is required to restore data from the backup.
    An encrypted
    FTSS_Backup.7z
    file is created and included in the
    FactoryTalk Services Platform
    Backup.
  4. Verify that the backup file is present in this location
    C:\ProgramData\Rockwell\RNAServer\Global\RnaStore\FTSS_Backup
    TIP: The
    ProgramData
    folder is hidden by default in
    Windows
    File Explorer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal