Select multiple table rows

Select multiple rows in a table to perform actions on multiple items.
  1. From the navigation bar, select either
    Zones
    ,
    Conduits
    , or
    Devices
    .
  2. Select a row by selecting a cell in the first column of a row.
  3. Either:
    • To add a row to the current selection, press
      +
      .
    • To continue the selection upward, press
      +
      .
      TIP: If the selection moves over a previously selected row, it deselects that row.
    • To continue the selection downward, press
      +
      .
      TIP: If the selection moves over a previously selected row, it deselects that row.
    • To select all rows between the previously selected row and the last selected row, press
      +
      .
SHARED PROPERTIES
pane displays.
You can do the following on a multiple-row selection:
  • View properties common to all selected items in
    SHARED PROPERTIES
    .
  • Change the common properties of all selected items in
    SHARED PROPERTIES
    .
    TIP:
    • The values that are identical across all selected items are displayed.
    • The properties are editable even if no value is displayed.
    • Checkboxes display a hyphen
      [-]
      when only some items have a property selected.
  • Delete
    selected items.
  • Edit
    selected zones.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal