Install or update software

Install or update
FactoryTalk Policy Manager
and
FactoryTalk System Services
with a graphical user interface (GUI) installer.
TIP: To install software from the command line, see Unattended or silent install.
IMPORTANT:
The
FactoryTalk Policy Manager
installation agent opens these Windows Firewall ports:
UDP 5353
and
TCP 40014
. To operate correctly, the Automatic Policy Deployment functionality requires these ports to be open.
Automatic Policy Deployment uses the Enrollment over Secure Transport (EST) service. If your machine has multiple network interfaces, the EST service uses a random network interface by default. You can select a specific network interface by editing the
appConfiguration.json
file. You must be a Windows administrator and have a FactoryTalk Directory administrator account to specify the network interface for the EST service.
  1. To install or update
    FactoryTalk Policy Manager
    and
    FactoryTalk System Services
  2. Close all open programs.
  3. Run the
    FactoryTalk Policy Manager
    installer and follow the installation wizard steps.
  4. (optional) To add or remove the components that you want to install, select
    Customize
    .
  5. Select
    Install
    .
  6. Read and agree to the EULA.
  7. Complete the installation.
  8. Restart the machine.
IMPORTANT:
FactoryTalk System Services
start automatically after a few minutes when you restart your computer. During that time, you cannot use
FactoryTalk Policy Manager
.
If
FactoryTalk System Services
do not start automatically, see Start FactoryTalk System Services.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal