Run a
FactoryTalk® Optix
Application in a
ThinManager®
Container

ThinManager®
version 14.1 and later includes a
FactoryTalk® Optix
container, which can be used to host an Optix application directly on a
ThinManager®
-managed thin client. Applications deployed for use with the new
ThinManager®
Optix Container support both the Native Presentation Engine and the Web Presentation Engine.
We recommend you design and test your Optix application within
FactoryTalk® Optix Studio
as normal. Then export the application from
FactoryTalk® Optix Studio
, and import it into the
ThinManager®
Admin Console.
For more information, see the
ThinManager®
14.1 Thin Client Management Platform User Manual, publication TM-UM001
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal