FactoryTalk® Optix Studio
Applications as Container Solution

FactoryTalk® Optix Studio
Applications can run containerized in two ways.
  • Build your own Docker container
  • Use
    ThinManager®
    containers to run web-based applications and
    FactoryTalk® Optix
    Applications on thin clients without additional server computers.
    ThinManager®
    is Rockwell Automation’s content delivery and thin client management software platform.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal