Open or download a release
Open the desired
FactoryTalk® Optix™
release or download a current or
previous FactoryTalk® Optix™
release from the FactoryTalk® Optix™
landing page.- Access theFactoryTalk® Optix™landing page. See FactoryTalk Optix landing page.
- When theFactoryTalk® Optix™landing page opens, the main page is set to theReleasessection.
- In the list of releases, navigate to the required release or enter the release number inSearch.
- Next to the release, select either:
- Open in Browser: The selectedFactoryTalk® Optix™release opens in a browser.
- Download: Complete the download by following the steps as described in FactoryTalk Optix Studio setup.
Provide Feedback