Calculate the size of your Runtime
The
Runtime Sizing
calculator determines the suitable FactoryTalk® Optix™
Runtime package in tokens that is required for your
application. To access the
Runtime Sizing
section of the FactoryTalk® Optix™
landing page:- Select theRuntime Sizingtab.
Before purchasing a
FactoryTalk® Optix™
Runtime entitlement, determine its size. Complete the wizard to determine the recommended package size for your application. As you complete the wizard, the top of each page displays an updated number of tokens and consequently a recommended package size from XS to XL.- Select presentation: Select either or bothNative HMI Client (1 token)andWeb HMI Client. UnderHow many sessionsselect the number of sessions (tokens), then selectNext.TIP: ANative HMI Clientpresentation includes all of the classic controls data, images, and drawings. AWeb HMI Clientpresentation includes those same items and makes them accessible from one or multiple HTML5 web clients.
- Select features: Select the features that you wish to use in your application. Select eitherSelect All (# tokens),None, or any individual features and then selectNext.
- Controller connections: Select one or more controllers to which you would like to establish a single or multiple connection, and then selectNext.
- InSelect interoperability, configure theOPC UA clientandOPC UA serverarchitecture as required, and then selectNext.
- SelectPreview and purchaseto view a summary of your selections and the final recommended package size for purchase.
- UnderRuntime Package and Support Options, select a support option.
- To upgrade your Runtime option from the recommended size to the following one, select the size option that you wish to purchase underUpdgrade to Station Runtime Lite (x) (x tokens)TIP:(x) (x tokens)may vary depending on requirements.
- Once you have determined the required Runtime package size, you can purchase the entitlement on the Commerce Portal. To make this easier, selectCopy Catalog Numberto copy the selected catalog number to the clipboard. You can then paste the catalog number into the Commerce Portage search bar or any required document. To open the Commerce Portal, selectPurchase FactoryTalk Optix.Commerce Portal opens the page where you complete your purchase.
- Log in, then paste the catalog number into the search bar. Select
to add the catalog number to your cart.
Provide Feedback