Step by step Setup Guide
- Check System requirements and see FactoryTalk Optix architecture.
- To access yourFactoryTalk® Optix™application you must access FactoryTalk Hub first. To access FactoryTalk Hub, you must Create your MyRockwellAutomation account.
- To useFactoryTalk® Optix™, you must belong to aFactoryTalk® Hub™organization. See Join or create a FactoryTalk Hub organization.TIP: A company is typically associated with an organization that company users can join. All of the entitlements activated for a company are allocated to the organization.
- Configure yourFactoryTalk® Optix™Studio:
- Start your configuration with the Initial settings on theFactoryTalk® Optix™Landing page.
- To download your locally installed FactoryTalk Optix Studio or access your cloud-enabledFactoryTalk® Optix™Studio, see FactoryTalk Optix Studio.
- (optional) Set up aFactoryTalk® Optix™Pro entitlement:IMPORTANT:FactoryTalk® Optix™Studio Pro entitlements are assigned to specific users, whereasFactoryTalk® Optix™Runtime entitlements are assigned to a specific Runtime device.
- Start FactoryTalk Optix Studio Pro and log in using your MyRockwellAutomation account.
- Select the Organization that you previously associated with your account and for which you purchased an entitlement.
- Set up a Runtime entitlement:
- Calculate the size of your Runtime by using the Runtime Sizing calculator.
- Access the Entitlements Landing page section to purchase, allocate and activate a Runtime entitlement as described in the FactoryTalk Optix Runtime setup section.
- Once you have created your application, use the Device Sizing calculator to identify the optimal device to run yourFactoryTalk® Optix™application.TIP: To create your application, refer to the Basic concepts and Tutorials sections of the FactoryTalk Optix Help.
Provide Feedback