Join or create a FactoryTalk®
Hub™ organization
FactoryTalk®
Hub™
organizationFactoryTalk®
Hub™
requires an organization in order to work with an
application.When selecting the
symbol appears in the upper right corner of the tile if no organization is
selected or if your account is not allowed to access
FactoryTalk®
Optix™
tile, a
symbol appears in the upper right corner of the tile if no organization is
selected or if your account is not allowed to access FactoryTalk®
Optix™
.
TIP:
If you are working with
FactoryTalk Optix Pro
, you may
want to set up an organization for FactoryTalk Remote Access
too. Refer to the FactoryTalk Remote Access
user guide for further
information on this topic.
TIP:
Verify that you selected the correct organization when you log into
FactoryTalk®
Hub™
. The organization name appears on the right side of the
FactoryTalk®
Hub™
title bar. If you have access to more organizations, you can
toggle from one to another by selecting the organization name.
The user that creates an organization becomes the organization owner and administrator. A
company may be associated to one or more organizations whose administrators can invite users
to join them. Once a user joins and selects an organization on
FactoryTalk®
Hub™
, the lock on the FactoryTalk®
Optix™
tile disappears and FactoryTalk®
Optix™
becomes accessible through the tile.- To create an organization, in theFactoryTalk® Hub™page title bar, select
and then select Create Organization. - On theSetup Your Organizationpage, complete:
- Name of the Organization: Enter the organization name.
- Location: Enter the organization location.
TIP: If you access the organization with owner or administrator rights, you can invite other users to join the organization, assign users to the organization and manage their permissions. You can also assign the administrator role to other users.TIP: You can allocate an entitlement fromFactoryTalk® Hub™to an organization if you are the owner of the entitlement without being the organization owner too. Once the owner allocates both the Studio Pro and Runtime entitlements to an organization, any user accessing that organization can self-assign any Studio Pro entitlements and use any Runtime entitlement key. - (optional) To determine if you want your organization to be visible in the public list, select eitherShow this organization in the public list and in search resultsorHide this organization in the public list and in search results, invite code required for members to join.TIP: Administrators must approve new members that are joining a public organization.
- SelectNext.
- Select whichFactoryTalk® Hub™applications you want visible to your organization and its members.TIP: All applications are visible by default.
- SelectCreate.A notification appears confirming that your organization is successfully created.IMPORTANT: A 90-day trial entitlement is automatically created for your new organization for bothFactoryTalk® Optix Studio™Pro andFactoryTalk® Remote Access™.
- In the upper left corner of theFactoryTalk® Hub™page, selectHome.TIP: Trial entitlement association takes a few minutes, so you may still see
on the FactoryTalk® Optix™andFactoryTalk® Remote Access™tiles. Refresh your screen until
no longer appears on those
tiles. - (optional) To invite other users to join your organization:
- In theFactoryTalk® Hub™page title bar, select
and then select
Invite Users. - UnderInvite by email, inResource, select the drop-down arrow and then selectService: FactoryTalk Optix.
- InRole, select the drop-down arrow and then select the role of the users that are going to be added to the organization.
- InEmail, type the email addresses of the invitees, separating each invitee with a semicolon.
- SelectSend Invite.TIP: You can share a link to invite the recipients to join the organization instead of entering resource and role:
- Underor share a joint request link, selectCopyto copy the link.
- Paste the link into an email addressed to the organization invitees.
Provide Feedback