CLI command: open
Use the
open
command to open a project in FactoryTalk Optix Studio
.Syntax
"C:\Program Files\Rockwell Automation\FactoryTalk
Optix\
version
\FTOptixStudio" open
project_to_open
[--silent]Parameter | Importance | Description |
|---|---|---|
version | Required | Folder name that reflects the installed FactoryTalk Optix Studio version. |
project_to_open | Required | Path to the OPTIX file of the project to
open. |
--silent | Optional | Make the command output non-verbose in the command prompt. |
Example
"C:\Program Files\Rockwell Automation\FactoryTalk Optix\Studio
1.6.0.626\FTOptixStudio" open
"D:\temp\NewHMIProject28\NewHMIProject28.optix"
Provide Feedback