CLI command: new

Use the
new
command to create a project.

Syntax

"C:\Program Files\Rockwell Automation\FactoryTalk Optix\
version
\FTOptixStudio" new
project_to_create
path
[-e | --encrypt-secrets] [--template=
template
] [--main-window-width==
width
] [--main-window-height==
height
] [-l | --in-project-location] [--silent] [-u | --user-defined-templates] [-d, --default-template-dimensions]
Parameters
Parameter
Importance
Description
version
Required
Folder name that reflects the installed
FactoryTalk Optix Studio
version.
project_to_create
Required
Name for the project.
path
Required
Location for the project.
-e
or
--encrypt-secrets
Optional
Encrypt secrets in the project.
--template=
template
Optional
Name of the template to use for the project.
The allowed values for
template
are:
  • main
    (default)
  • optixPanel
--main-window-width=
width
Optional
Width for the main window in pixels. The default width is
400
pixels
--main-window-height=
height
Optional
Height for the main window in pixels. The default height is
400
pixels
-l
or
--in-project-location
Optional
Create the project directly under
path
--silent
Optional
Make the command output non-verbose in the command prompt.
-u, --user-defined-templates
Optional
The project template is a user-defined template
-d, --default-template-dimensions
Optional
Use default template dimensions when creating the new project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal