Configure an external event
Add an external event to an object. An external event may be an event from another
object. Adding an event from an object to another object enables you to avoid recreating the
same event for multiple objects.
- FromProject view, select the object that you want to contain the external event.
- InPropertiesnext toEvents, select
Add external event. - Select the event to manage the events of another object.
- ChooseSelect.The new event appears underEvents.
- If needed, link methods to the external event.For more information, see Add a method to an existing event.
custom event
Provide Feedback