Create remote panel (types)
Create a panel type that will be used on client.
- Create a folder for remote panels:
- InProject view, right-click theUIfolder and select .
- Hover-over the folder, select, and enter
RemotePanels.
- Create the main panel:
- InProject view, right-clickRemotePanelsand select .
- Hover-over the pane, select, and enter
MainPanel.
- Create a panel that displays the Speed variable:
- InProject view, right-clickRemotePanelsand select .
- Hover-over the pane, select, and enter
SpeedPanel.
- Create a panel that displays the Acceleration variable:
- InProject view, right-clickRemotePanelsand select .
- Hover-over the pane, select, and enter
AccelerationPanel.
Provide Feedback