FactoryTalk Linx Data Bridge activations
The activation type determines the feature support of the
FactoryTalk Linx Data Bridge
.FactoryTalk Linx Data Bridge
version 6.21.00 adds the ability to allow users to choose the specific activation that will be requested on startup. Find the available activations from General Settings
> Activation to be utilized
.If .
FactoryTalk Linx Data Bridge
fails to detect a valid activation file, an error is logged to FactoryTalk Diagnostics
, and FactoryTalk Linx Data Bridge
operates under a grace period. For more information about grace periods, see FactoryTalk Services Platform
HelpActivation Name | Activation | FactoryTalk Directory | Activates FactoryTalk Linx Data Bridge | Supported Data Pairs | ||
|---|---|---|---|---|---|---|
FactoryTalk Linx Gateway Professional | LINXGW.PROFESSIONAL | Local or Network | Y | 200,000 | ||
FactoryTalk Linx Data Bridge | LINX.DATABRIDGE | Local or Network | Y | 2,000 | ||
FactoryTalk Linx Data Bridge Embedded | Verifies its operating on a CompactLogix™ 5480 windows core | Local or Network | Y | 500 | ||
TIP:
The Activation type is only shown when the pair tag is configured or added.
Provide Feedback