Add individual Historian points
Use the
Add Individual Historian Points
dialog to add individual Historian points to
a FactoryTalk Historian SE
server.To add points to a server
- In the Explorer window of theFactoryTalk® Administration Console, right-click the FactoryTalk application from which you want to collect points, and then selectAdd Individual Historian Points.
- In theAdd Individual Historian Pointsdialog, configure the following:SettingDescriptionHistorian serverSelect the appropriateFactoryTalk Historian SEserver to which you want to add points.Data collection interfaceSelect the appropriate interface for data collection.From applicationSelect the application from which you want to collect points.Tag attributes configurationSelect the tag attributes file from which you assign the tag attributes to the new points.Configuration file editorOpen theFactoryTalk Historian Discovery Rule Editordialog in which you can edit the tag attributes file by selectingTag Attributes Setting.Default scan rateSelect the interval at which you want to collect points.
- SelectBrowse tagsto open the Tag Browser.
- Locate the tags that you want to add to the server and selectConfirm.The tags are added to the right pane of theAdd Individual Historian Pointsdialog.
- Select the checkboxes next to the Historian points that you want to add, and then selectConfirm points.
indicates that the Historian point has been added to the FactoryTalk Historian SEserver successfully.
indicates that the Historian point failed to be added to the FactoryTalk Historian SEserver. Hover over this error icon to see the error messages.
- SelectCloseto return to theFactoryTalk Administration Console.
Provide Feedback