Update the known servers table
The known servers table (KST) contains a list of Data Archive servers and Asset Framework
(AF) servers used by client applications for connections. Previously, AF servers were
stored in a file, while Data Archives were stored in the Windows registry. Starting with
PI AF Client 2024, AF SDK applications now store the entire KST in local files instead
of the registry.
- If FactoryTalk Historian Asset Framework is installed:
- Go to theStartmenu and openSystem Explorer.
- Create anAsset Frameworkdatabase.
- ExpandFile>Connections, and then selectAdd Data Server.
- Add the Historian SE server's hostname that you want to create Historian server connections.
- If FactoryTalk Historian Asset Framework is not installed:
- Run the following command-line:"%PIHOME64%AF\KSTMigrationTool.exe" /forceoverwrite
Provide Feedback