2.03.00
July 2026
New Features
- New Enterprise and Regional Dashboards with Global Map Overview: Enterprise and Regional dashboards now include an interactive global map that displays all sites worldwide. Users can quickly visualize and compare key EnPI, including Harmonized Energy, Cost, Emissions, and Energy Intensity to identify high-energy-use regions, benchmark site performance, and prioritize efficiency improvements.
Enhancements
- Timezone Improvements: This enhancement extends time zone support across Notifications, Reports, Analytics, and all EnPI-related services. All time-dependent data is stored consistently in UTC while being displayed, calculated, and processed according to the configured site time zone or user time zone.
- Improved Retrospective Calculations: This enhancement enables accurate retrospective recalculation of energy, cost, emissions, and all derived energy performance indicators (EnPIs) when historical rate schedules, emission factor schedules, baselines, or system configurations are updated.
- Collapsible Energy Model Hierarchy: The energy model hierarchy tree now supports expand and collapse behavior, making it easier to navigate and manage large energy model structures with numerous regions, sites, areas, and meters.
- Meter-Level Icons: Updated icons are now displayed at the meter level in the energy model hierarchy and navigation menu, providing improved visual representation and usability for distinguishing between different meter types.
- Improved Chart Tooltips with Timestamps: Chart tooltips across dashboards have been enhanced to display accurate timestamps, providing additional context and data precision when hovering over data points in consumption, demand, cost, and emissions charts.
Fixed Anomalies
- Fixed an anomaly where the downloaded Measurement and Verification (M&V) project report displayed data in the previously set units even after applying the updated unit conversions configured in the application. [4944284]
- Fixed an anomaly where site dashboard charts showed duplicate Y-axis labels when the time scope was set to Monthly. [5004428]
- Fixed an anomaly where the dashboard displayed incorrect Previous Period values on the first backwards navigation for the time scopes: Last Hour, Last 8 Hours, Last 48 Hours, and Last 72 Hours. [5297326]
- Fixed an anomaly where the application did not apply the Emissions Factor to the current (actual) period or to historical (retrospective) periods. [5562448]
- Fixed an anomaly where the Sankey diagram on the Distribution tab showed energy and consumption values that did not match the meter-level values.
- Fixed an anomaly where the dashboard showed values one day ahead on the day of a schedule change. This issue occurred when the browser used a local time zone and the rate schedules and emission factors used multiple time slots. [5671677]
- Fixed an anomaly where the charts in the Consumption & Demand, Emission, and Cost reports plotted values incorrectly for all time scopes (Day, Week, Month, and Year). [5681970]
- Fixed an anomaly where meters showed a datalink error after meter creation, although the datalink mapping was configured correctly. [5684151]
- Fixed an anomaly where the Sankey distribution diagram did not always draw the lines that connect the site total to the sub-meters when the user switched between sites more than once. [5686586]
- Fixed an anomaly where theFactoryTalk® Energy Manager™calculated tags (Time of Use, Energy Cost, and CO2Emission) did not generate data for four days because the organization'sFactoryTalk® Hub®entitlements had expired. The expired entitlements made FactoryTalk Energy Manager andFactoryTalk® DataMosaix™inactive, and the dashboards showed no values. Once the user renewed the FactoryTalk Hub license, the calculated tags generate data and display values in the dashboards. [5770248]
- Fixed an anomaly where the Region and Enterprise roll-ups did not aggregate the site-level data, although the site-level dashboards showed correct values and the data link worked correctly. [5770277]
- Fixed an anomaly where the demand chart showed no data on the dashboard for a Steam meter, although the data existed and appeared in the datalink preview chart. [5774561]
Provide Feedback