Ladder Diagram Safety Instructions
Routines in the safety task can use the following types of ladder diagram safety
instructions.
When instructions that result in values with decimal place are used with REAL or LREAL
operands,
Rockwell Automation®
has verified the precision to six decimal
places.Advanced Math
Rockwell Automation®
has not done independent mathematical analysis of the
numerical algorithms that are used in any of the following advanced math instructions. If
you require a specific degree of accuracy, you must functionally test this instruction over
your expected input domain.Mnemonic | Name | Description |
|---|---|---|
EXPT | X to the Power of Y | Returns the value of X to the power of Y. |
LN | Natural Log | Compute the natural log of a number. |
LOG | Log Base 10 | Compute the log base 10 of a number. |
Array (File)
Mnemonic | Name | Description |
|---|---|---|
AVE | File Average | Calculate the mean/average over a set of values. |
COP | Copy File | Copy binary data from one tag to another (no type conversion). When you use the COP instruction in a safety routine, you must verify that the
length is a constant and that the source and destination length are the same. |
FAL | File Arithmetic and Logic | Perform copy, arithmetic, logic, and function operations on data that is stored
in an array. |
FLL | File Fill | Fill the elements of an array with the source value, while leaving the source
value unchanged. |
FSC | File Search and Compare | Compare the values in an array, element by element. |
SIZE | Size in Elements | Find the size of a dimension of an array. |
STD | File Standard Deviation | Calculate the standard deviation over a set of values. |
BSL | Bit Shift Left | Shifts the specified number of bits to the left. |
BSR | Bit Shift Right | Shifts the specified number of bits to the right. |
FFL | FIFO Load | Store a value into an array by using first-in/first-out semantics. |
FFU | FIFO Unload | Retrieve a value from an array by using last-in/first-out semantics. |
LFL | LIFO Load | Store a value into an array by using last-in/first-out semantics. |
LFU | LIFO Unload | Retrieve a value from an array by using last-in/first-out semantics. |
Bit
Mnemonic | Name | Description |
|---|---|---|
ONS | One Shot | Allows an event to occur one time on false-to-true edge of rung state. |
OSR | One Shot Rising | Sets an output bit for one scan on the false-to-true (rising) edge of rung
state. |
OSF | One-Shot Falling | Sets an output bit for one scan on the true-to-false (falling) edge of rung
state. |
OTE | Output Energize | Controls a bit (it performs both Set and Clear operations that are based on rung
state). |
OTL | Output Latch | Set a bit (retentive). |
OTU | Output Unlatch | Clear bit (retentive). |
XIC | Examine if Closed | Examines the data bit to set or clear the rung condition. |
XIO | Examine if Open | Examines the data bit to set or clear the rung condition. |
Timer/Counter
Mnemonic | Name | Description |
|---|---|---|
CTD | Count Down | Count down. |
CTU | Count Up | Count up. |
RES | Reset | Reset a timer or counter. |
RTO | Retentive Timer On | Accumulate time. |
TOF | Off-delay Timer | Time how long a timer is disabled. |
TON | On-delay Timer | Time how long a timer is enabled. |
Compare
Mnemonic | Name | Description |
|---|---|---|
EQ | Equal To | Test whether two values are equal. |
CMP | Compare | Perform a comparison on the arithmetic operations that you specify in the
expression. |
GE | Greater Than Or Equal To | Test whether one value is greater than or equal to a second value. |
GT | Greater Than | Test whether one value is greater than a second value. |
LE | Less Than or Equal To | Test whether one value is less than or equal to a second value. |
LT | Less Than | Test whether one value is less than a second value. |
LIMIT | Limit | Test whether a value falls within a specified range. |
MEQ | Mask Equal To | Pass source and compare values through a mask and test whether they are
equal. |
NE | Not Equal | Test whether one value is not equal to a second value. |
Move/Logical
Mnemonic | Name | Description |
|---|---|---|
AND | Bitwise AND | Perform bitwise AND operation. |
CLR | Clear | Clear a value. |
MOVE | Move | Copy a value. |
MVM | Masked Move | Copy a specific part of an integer. |
NOT | Bitwise Not | Perform bitwise NOT operation. |
OR | Bitwise Or | Perform bitwise OR operation. |
SWPB | Swap Byte | Rearrange the bytes of a value. |
XOR | Bitwise Exclusive Or | Perform bitwise exclusive OR operation. |
Program Control
Mnemonic | Name | Description |
|---|---|---|
AFI | Always False Instruction | Forces a rung to false (rung continues to execute). |
EventTrigger | Trigger Event Task | Triggers one execution of an event task. |
JMP | Jump To Label | Scan of logic jumps to a labeled location within the same routine. |
JSR | Jump to Subroutine | Jump to a separate routine. |
LBL | Label | Identifies a target location for a JMP instruction. |
MCR | Master Control Reset | Forces every rung in a section of logic to execute in the False state. |
NOP | No Operation | Insert a placeholder in the logic. |
RET | Return | Return the results of a subroutine. |
SBR | Subroutine | Accept data that the JSR instruction passes to a subroutine. |
TND | Temporary End | Mark a temporary end that halts routine execution. |
Safety
ATTENTION:
Safety application instructions are the only
instructions that can be used in the safety task for SIL 2 or SIL 3 applications.
Mnemonic | Name | Description |
|---|---|---|
CROUT | Configurable Redundant Output | Controls and monitors redundant outputs. |
DCM | Dual Channel Input - Monitor | Monitors dual-input safety devices. |
DCS | Dual Channel Input Stop | Monitors dual-input safety devices whose main purpose is to provide a stop
function, such as an E-stop, light curtain, or gate switch. |
DCSTL | Dual Channel Input Stop With Test and Lock | Monitors dual-input safety devices whose main purpose is to provide a stop
function, such as an E-stop, light curtain, or gate switch. It includes the added
capability to initiate a functional test of the stop device. It can monitor a
feedback signal from a safety device and issue a lock request to a safety
device. |
SMAT | Safety Mat | Indicates whether the safety mat is occupied. |
Compute/Math
Rockwell Automation®
has done no independent mathematical analysis of the
numerical algorithms that are used in the SQRT or SQR instructions. If you require a
specific degree of accuracy, you must functionally test this instruction over your expected
input domain.Mnemonic | Name | Description |
|---|---|---|
ABS | Absolute Value | Take the absolute value of a value. |
ADD | Add | Add two values. |
CPT | Compute | Perform the arithmetic operation that is defined in the expression. |
DIV | Divide | Divide two values. |
MOD | Modulo | Determine the remainder after one value is divided by a second value. |
MUL | Multiply | Multiply two values. |
NEG | Negate | Take the opposite sign of a value. |
SQRT | Square Root | Calculate the square root of a value. |
SUB | Subtract | Subtract two values. |
Trigonometric
Rockwell Automation®
has not done independent mathematical analysis of the
numerical algorithms in any of the following trigonometric instructions. If you require a
specific degree of accuracy, you must functionally test this instruction over your expected
input domain.Mnemonic | Name | Description |
|---|---|---|
ACOS | Arc Cosine | Compute the arc-cosine of a number. |
ASIN | Arc Sine | Compute the arc-sine of a number. |
ATAN | Arc Tangent | Compute the arc tangent in radians of y/x based on the sign of a value to
determine the correct quadrant. |
ATAN2 | Arc Tangent 2 | Compute the arc tangent in radians of y/x based on the signs of both values to
determine the correct quadrant. |
COS | Cosine | Compute the cosine of a number. |
SIN | Sine | Compute the sin of a number. |
TAN | Tangent | Compute the tangent of a number. |
Math Conversion
Mnemonic | Name | Description |
|---|---|---|
DEG | Degrees | Convert radians into degrees. |
BCD_TO | Convert to Integer | Convert the BCD value to an integer value. |
RAD | Radian | Convert degrees into radians. |
TO_BCD | Convert to BCD | Convert the integer value to a BCD value. |
TRUNC Truncate Remove the fractional part of a value. | Truncate | Remove the fractional part of a value. |
Provide Feedback