Minor Firmware Revision Match
When you deploy a signed application,
FactoryTalk® Design Studio™
checks the minor
firmware revision used to generate the safety signature to be reapplied. If the minor
firmware revision in the project is different than the minor firmware revision running
in the safety controller, a notification message appears. After an authorized safety
user acknowledges the message, FactoryTalk® Design Studio™
removes the safety
signature before deploying the application to the safety controller.Provide Feedback