Sort tags
Sort columns to see the tags of interest in the item. Select the heading of a column in Tag
Editor to sort the tags by the values in that column.
- On the explorer, go to the
Systemview, the
Executionview, or the
Libraryview. - Right-click a controller, a program, a routine, or an add-on instruction, and then selectTags and parameters.TIP: You can also select
View tags and parameters: (item name). - In the Tag Editor column to sort, select either:
. Sort the tags in ascending order based of the values in the column.
. Sort the tags in descending order based of the values in the column.
Provide Feedback