Configure a grid

Configure a grid or table to show or hide data. For example, show only the columns in the Tag Editor so the grid contains only the data you want to see. Do this to more quickly determine the tag values used in a manufacturing system.
To configure a grid
  • Hide a column
    . Right-click a column heading and select
    Hide column
    . The column does not appear in the grid.
  • Show a column
    . Right any column heading, select
    Toggle column
    , and then select the column to show. The column appears in the grid.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal