Tag Editor
The Tag Editor shows all tags for a controller, a program, a routine, or an add-on
instruction. The Tag Editor shows the name, data type, usage, value, style, description, and
connections for each tag. Use the Tag Editor to:
- Add a tag.
- Edit a tag or parameter.
- Delete a tag.
- View, add, edit, and delete parameter connections. Refer to Program parameter connections.
Provide Feedback