Structured Text Editor toolbox

Use the Structured Text
Toolbox
to add elements and instructions to the ladder diagram. If the
Toolbox
is not open when you open the ladder diagram routine, select Toolbox
Toolbox
.
Select the icon on the Structured Text
Toolbox
to add elements to the routine:
Icon
Adds
If statement icon
If statement
Case statement icon
Case statement
For statement icon
For statement
While statement icon
While statement
Repeat statement icon
Repeat statement
The
Toolbox
also displays the categories of instructions you can add to the routine.
Search
in the
Toolbox
displays elements to add to the routine without having to navigate the categories of the
Toolbox
. As soon as you start typing an element name, elements that contain the search text appear in the
Toolbox
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal