Create tags in the Structured Text Editor
Create tags in the Structured Text Editor as you build a routine.
To create tags in the Structured Text Editor
- On a line in the routine, add an instruction or a statement.The inline guide dialog indicates the parameters required and describes the type of tag required for each. For example, the inline guide for a COP instruction indicates required Source, Dest, and Length parameters.Inline guide example

- Type a name for a tag, such as myBit. The AutoComplete dialog lists tags that can be referenced from the routine. If the tag you need is listed, select it.AutoComplete example

- If an existing tag is not available, type a tag name, right-click on it, and selectCreate new tagto open theCreate new tagdialog.In the Create New Tag dialog, enter the required settings and selectCreate. See Create a tag for more information on tag settings and requirements.
Provide Feedback