Generate a safety confirmation report
Generate a safety confirmation report for a safety project. Use the report to
verify the safety project.
For more information on confirming and verifying safety projects, see the
Develop
Safety Applications in FactoryTalk Design Studio Programming Manual
(publication
FTDS-PM001).- Go online with the safety controller.
- On the explorer bar, select
Execution. - Right-click a safety project, and then selectGenerate safety confirmation report.TIP: Report generation might encounter issues for projects with a large number of tags. If the total exceeds 300,000, consider reducing the number of tags and try again.FactoryTalk Design Studiogenerates the report and displays it.
- (optional) SelectDownloadto save the report as a PDF file.
Provide Feedback