Reset a cloud-hosted emulated controller
FactoryTalk Design Studio
allows a reset for emulated controllers at any time. In
most cases, FactoryTalk Design Studio
can automatically recover from connection
problems without requiring a reset. If automatic recovery fails, FactoryTalk Design Studio
displays the connection status on the
Output
pane and indicates that a reset is required.Resetting the emulated controller discards the current image and snapshot and creates a new
image.
- In thePathcolumn onDeploy center, selectReset.TIP: You can also selectReseton theOnlinepane.
Provide Feedback