Deploy to a cloud-hosted emulated controller
- On the top toolbar, select
to open
Deploy center.TIP: You can also selectDeploy centerat the bottom of theDevicesexplorer. - OnDeploy center, in thePathcolumn, select
, and then select Use emulator. - Select the checkbox for the controller application, and then selectDeploy.
- InDeployment warning, selectContinue.A progress bar indicates the status of the current build and deployment for the controller.
- InChoose a controller to go online with after deployment ends, select a controller, and then selectOK.TIP: You can be online with only one controller at a time. If you are currently online with a controller and choose to go online with a different controller, you automatically go offline with the current controller and all monitoring tabs are closed.
Provide Feedback