Delete a project
Delete a project from the
Open project
dialog.- Close any open project.
- Open theOpen projectdialog by doing one of the following:
- On theWelcomepage, selectOpen project.
- From the menu bar, select .
- In theOpen projectdialog, do the following:
- InOpen from, selectLocal.
- InProject name, hover over the project that you want to delete, and then select
.
The user's copy of the project is deleted. The shared project and any other user copy of the
project will still exist.
Provide Feedback