Add-On Instructions
Add-On Instructions are best used for encapsulating and reusing complex logic. They allow you to create a self-contained block of logic that can be used multiple times within a program, improving code readability and maintainability.
Add-On Instructions are commonly used for:
Modularizing Code
. Add-On Instructions help break down complex programs into smaller, manageable modules. This makes it easier to troubleshoot and update specific parts of the program without affecting the system.Improving performance
. By encapsulating logic, Add-On Instructions can reduce the amount of code that needs to be executed during each scan cycle to help improve performance.Reusability
. Add-On Instructions can be used across different projects to save development time and ensure consistency in logic implementation.Simplifying maintenance
. Add-On instructions help manage and maintain code to ensure changes in logic only need to be made in one place. Add-On Instruction can be used by any controller application in a project and enable reuse between different controller applications. Define the instructions, use instructions provided by another user, or copy instructions from another project. Once defined in a project, Add-On Instructions behave like built-in instructions in
FactoryTalk Design Studio
. Add-On Instructions are commonly used to represent reusable blocks of common code. FactoryTalk Smart Objects are used to represent hierarchical designs of your system.
Add-On Instructions can contain a maximum of 2 megabytes of data.
Add-On Instructions allow you to:
Reuse Code |
|
Provide an understandable interface |
|
Simplify maintenance | Simplify code maintenance by viewing tag values relative to a specific
instance of an Add-On Instruction. |
Provide Feedback