Role permissions

Permissions allow a user to perform certain tasks. The permissions displayed depend on the role selected. Permissions for predefined roles are read-only. Predefined roles include:
  • Admin
  • Engineer
  • Guest
  • Safety Engineer
You can assign permissions for a role when creating or updating a custom role. The user of an assigned role has the permissions to perform the indicated tasks. Roles for a feature appear grouped by category:
Category
Permission
Description
User Role Management
Update
Update user roles in
Role Management
.
Project
Save As
Duplicate a project and save it with a unique name.
Deploy
Deploy a controller application to a controller device.
Go Online
Go online with a controller.
Push
Push changes to the project to a remote repository.
Share across Organizations
Copy a project to a different organization.
Safety
Edit
Edit safety content in the project such as configuring a controller or device for safety content.
Lock
Lock a safety controller to protect the safety signature and prevent the deployment of safety changes.
Unlock
Unlock a safety controller to remove protection from the safety signature and allow the deployment of safety changes.
Generate Signature
Generate a safety signature to run a controller with safety integrity.
Delete Signature
Delete a safety signature to run a controller without safety integrity.
User-Defined Library
Share
Share user-defined libraries within the organization and delete libraries that the user has shared.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal