Tag syntax guidelines

Follow these guidelines when defining a tag.
  • The data type of the tag must come before the name of the tag.
  • When no value is specified, the default values for tags are defined by the data type.
    • Alias tags cannot set the default value.
  • FactoryTalk Design Studio applies these rules when writing out tags:
    • If there is a property on a tag, tag member, bit, or array element, a curly bracket contains the property. For example:
    • For tag members, if there is no property on the parent of the member, then no curly bracket is used. For example:
tag dint MyTag { desc := “hello”; }
tag timer mytimer {
len := 10;
pre {
desc := “desc on pre”;
} := 10;
}
tag timer mytimer {
len := 10;
pre.1 {
desc := “desc on pre.1”;
} := 10;
}
TIP:
Tips:
  • You can specify the values of a tag by using [tag name] := [value].
  • Specify properties and member values using this notation:
    { [property] := [value] }
  • Use this shortcut to set properties and values of tag members:
    { [member<.submember(s)>][.property] := [property value] }
    { [member<.submember(s)>] := [value] }
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal