Tag attributes
This table describes attributes in tag syntax.
Attribute | Description |
|---|---|
Name | Name of the tag. |
TagType | Specifies the tag as Base, Alias, Produce, or Consumed. |
DataType | The data type of the tag, such as BOOL, SINT, INT, DINT, LINT, REAL,
or an add-on instruction data
type. |
AliasFor | Name of the base tag that the alias tag references. |
Dimensions | Number of dimensions in an array. |
Provide Feedback