Use a PC-based phase

After creating the PC-based phase executable, you must perform the following tasks:
  • Update the area model in
    FactoryTalk Batch Equipment Editor
  • Add the phase to your recipes using
    FactoryTalk Batch Recipe Editor
The following table indicates the relationship between the PC-based phase property and the area model. You must adhere to the rules shown here to allow for proper communication.
Relationship between the PC-based phase property and the area model
PC-based phase property
Area model
The OPC’s
Watchdog Item Access Path
PC-based phase’s
OPC Access Path for Tags
, as defined in
Visual Basic
, or other container, or the
Topic
property (changing one also changes the other)
PC-based phase
Name
property, as defined in
Visual Basic
, or other container
Equipment Module’s
Tag
name, as defined in
FactoryTalk Batch Equipment Editor
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal