Add the control to the project

Use MFC to add the control to the project.
To add the control to the project:
  1. In MFC, select
    Project
    >
    Add to Project
    .
  2. Select the
    Components and Controls
    option.
  3. Open the
    Registered ActiveX Controls
    folder.
  4. Select the
    Batch Phase Execution
    control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal