Unable to access instruction file
The XML schema requires that the contents of any instruction files must be included in the
XML file.
FactoryTalk Batch Equipment Editor
must access the
instruction file at the time of the export. If the instruction files cannot be accessed,
this error message displays and the export does not occur. 
Provide Feedback